AXIS#.PROFINET.SENSORRESLINEAR

Description

This command sets the resolution of the G1_XIST1 and G1_XIST2 sensor positions when using linear feedback. If set to 0 the resolution is 220 counts per motor pole pitch. Any non-zero value sets the resolution in nanometers per count.

Versions

Action Version Notes
Implemented 02-16-01-000  

General Information

Type Read/Write
Units

nm/count

Range 0 to 4294967295
Default Value 0
Data Type Integer
Stored in Non-Volatile Memory Yes

Variants Supported

PROFINET drives: AKD2G-SPP

Industrial Ethernet Information

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PROFINET.SENSORRESLINEAR

5229

Unsigned32

Read/Write

-